MITSUBISHI ELECTRIC Daha İyiye Yönelik Değişiklikler
Manufacturing

Automation in cement and heavy industry

09.10.20264 dakika okuma

Cement plant automation is not a single upgrade. It involves deciding which equipment needs better control, what production data teams need and how to introduce changes without disrupting operations. A practical starting point is to identify issues such as energy visibility, equipment availability or maintenance planning and define the project around it.

Where automation supports cement production across the plant?

In aggregates processing, automation supports equipment such as conveyors, crushers, pumps and fans. If a critical asset is unavailable, production may be affected. PLCs and other controllers oversee operational tasks, but existing systems may limit teams’ ability to adjust processes or use performance data.

Cement plants have their own process requirements. The right level of automation depends on each plant’s equipment, infrastructure and objectives. Teams should assess the controls and data already available, identify where they limit operational decisions, and define the scope of any upgrade. Requirements for cement kiln automation, for example, should be confirmed against plant-specific engineering information.

The operational priorities driving cement plant automation

Energy use, equipment availability and maintenance are three practical priorities when assessing automation in the cement industry.

Energy use and visibility


Quarries and aggregates plants use energy-intensive equipment, including crushers, pumps and conveyors. Collecting and analysing energy data can help teams assess consumption and identify areas for investigation. Possible approaches include:

  • frequency inverters,
  • energy monitoring,
  • analytical systems.

Monitoring is useful when it informs a decision, such as which equipment to examine or which energy hotspot to prioritise. A phased approach can help teams focus first on areas where better information may be most useful.

Availability and maintenance


Availability is the ratio of actual asset run time to planned run time, while utilisation reflects the proportion of time an asset is used. These measures describe different aspects of operations and should be interpreted in context.

Predictive maintenance uses diagnostic data and analytics to help teams anticipate maintenance needs or possible failure. It can inform maintenance planning around production schedules, but it does not replace physical maintenance. A cement plant predictive maintenance project should start with a clear question about what equipment or decision the data is intended to support.

Modernisation and support


Cement plant modernisation may involve legacy equipment and obsolescence. Planning may need to consider:

  • migration tools and engineering support,
  • equipment upgrades,
  • technical training,
  • service arrangements

These considerations help teams plan implementation and ongoing support. They do not replace the need to define the operational objective of the upgrade.

    Integrating automation into an existing cement plant

    Begin by assessing the control infrastructure and data available for the equipment and processes in scope. Establish what teams can control, what information they can access and where current limitations affect decisions.

    Then define an objective and choose an initial area of work, such as a critical asset, a bottleneck or an area with limited energy visibility. A phased approach can account for budget, operational priorities and lessons learned, while planning for engineering, maintenance, system migration and staff training.

    For a related perspective on industrial digital transformation in another sector, see digital transformation in automotive plants.

    Using production data to guide maintenance and energy decisions

    Energy and diagnostic data are valuable when they help teams make operational decisions. Energy data can support analysis of consumption and costs; diagnostic data can help assess equipment condition and plan maintenance.

    The concrete-production case study at Holcim illustrates how a defined operating problem can be addressed with drive technology. Raw-material transport trolleys carried loads of up to five tonnes on steep ramps. Hard starting and braking caused mechanical jerking and failures of brakes and six mechanical components. The counter-current braking method also meant that 18 kW motors consumed full power while lowering loads.

    Holcim, working with system integrator DWI Motion, replaced traditional starters with Mitsubishi Electric FR-A800E inverters and FR-XC regenerative modules. The inverter provided vector control for managing loads on an incline, while the regenerative module managed energy during downward movement and returned it to the supply.

    The reported result was a saving of 11 kWh per day for a single drive, or more than 3 MWh per year, with an estimated reduction of approximately one tonne of CO₂ emissions. This is a specific result for one application, not a forecast for other equipment or plants.

    Measuring the impact of an automation project

    Choose measures that match the project objective. Depending on the work, these may include:

    • energy consumption and cost;
    • asset availability and utilisation;
    • diagnostic information and equipment condition;
    • mechanical wear and maintenance requirements;
    • production interruptions;
    • energy recovery and system health, where available.

    Before an upgrade, establish what the plant can measure and which indicators will show whether the project addressed the original problem. For energy reduction, use data relevant to the equipment being changed; for availability, compare planned and actual run time. The available materials support a staged approach but do not prescribe universal targets for cement plants.

      FAQ section

      Which processes in a cement plant can be supported by automation?

      Automation can support assets such as conveyors, crushers, pumps and fans. Cement-specific applications depend on the plant’s systems and objectives.

      How can automation be introduced into an existing cement plant?

      Assess current controls and data, define an operational objective, then plan a phased upgrade that considers migration, engineering and staff training.

      What should a plant assess before upgrading its control systems?

      Review existing infrastructure, asset-level controls, data access, project objectives, budget and operational requirements.

      How can plant teams monitor energy use?

      Collect and analyse energy data, then use it to identify areas for investigation. The setup depends on the plant’s equipment and processes.

      What production data is useful when planning an automation project?

      Relevant data may include energy use, diagnostics, availability, utilisation and system health. Choose based on the project objective.

      How can automation help teams identify equipment issues earlier?

      Condition monitoring and predictive maintenance use diagnostic data to help detect faults and plan maintenance. They do not replace physical inspections or repairs.

      Which indicators should be tracked after an automation upgrade?

      Track measures linked to the objective, such as energy use, availability, utilisation, equipment condition and maintenance needs.


      Benzer Makaleler


      Konular

      Manufacturing